Gets the current
Condition cast to the requested type. Obsolete. Use
Keysight.SA.Vsa.EventRule.GetExtension``1 instead.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Function GetCondition(Of T As EventCondition)() As T |
| C++/CLI | |
|---|
public:
abstract T^ GetConditiongeneric<typename T>
();
where T: EventCondition |
Type Parameters
- T
- The type to which to cast the returned EventCondition.
Return Value
The current
EventCondition cast to the requested type, or null if the current
EventCondition is not of the requested type.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also