| Overload | Description |
|---|---|
| SetCondition<T>() | Changes the current Condition to the indicated type (if necessary) and returns an appropriately typed handle to the EventCondition object. Obsolete. Use Keysight.SA.Vsa.EventRule.SetExtension``1 instead. |
| SetCondition(Type) | Changes the current EventCondition to the indicated type (if necessary) and returns a handle to the EventCondition object. Obsolete. Use SetExtension(Type) instead. |
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)