Keysight 89600 VSA .NET API
MacroEventActionExtension Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.Vsa Namespace : MacroEventActionExtension Class


Glossary Item Box

Pause measurement and run the specified macro.

Syntax

Remarks

The macro is run on a separate thread from the measurement so it should call Agilent.SA.Vsa.Measurement.WaitForMeasurementDone before reading results or changing configuration for a measurement.

When there are multiple DataSources, the macro is run once for each Agilent.SA.Vsa.Measurement corresponding to the DataSources.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also