Keysight 89600 VSA .NET API
MacroName Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.Vsa Namespace > MacroEventActionExtension Class : MacroName Property


Glossary Item Box

Gets or sets the Agilent.SA.Vsa.Macro.Name of the macro from the current set of Agilent.SA.Vsa.Application.Macros.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property MacroName As String
C# 
public abstract string MacroName {get; set;}
C++/CLI 
public:
abstract property String^ MacroName {
   String^ get();
   void set (    String^ value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also