Keysight 89600 VSA .NET API
Mode Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.Vsa Namespace : Mode Class


Glossary Item Box

A class providing access to Mode properties and methods.

Syntax

Remarks

A Mode is a named, typed container that holds shared configuration (ModeConfiguration) and a logical view of the measurements it owns. It is parallel to Context.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 31.00

See Also