Keysight 89600 VSA .NET API
Create Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.Vsa Namespace > ModeCollection Class : Create Method


Glossary Item Box

Create a new Mode using the indicated ModeConfiguration type, using default Mode.Name.

Overload List

OverloadDescription
Create(Type)Create a new Mode using the indicated ModeConfiguration type, using default Mode.Name.  
Create(Type,String)Create a new Mode using the indicated ModeConfiguration type, with the supplied name.  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also