Keysight 89600 VSA .NET API
ModeCollection Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.Vsa Namespace : ModeCollection Class


Glossary Item Box

This collection contains the set of Mode objects currently loaded in the application.

Object Model

ModeCollection ClassMode ClassMode Class

Syntax

Remarks

Modes are created implicitly as well as explicitly: a measurement whose type requires a Mode creates and associates one, and a Mode is removed again once no measurement requires its ConfigurationType. An empty collection is therefore normal.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 31.00

See Also