Keysight 89600 VSA .NET API
ConfigurationType Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.Vsa Namespace > Mode Class : ConfigurationType Property


Glossary Item Box

Gets the type of this Mode's ModeConfiguration.

Syntax

Visual Basic (Declaration) 
Public MustOverride ReadOnly Property ConfigurationType As Type
C# 
public abstract Type ConfigurationType {get;}
C++/CLI 
public:
abstract property Type^ ConfigurationType {
   Type^ get();
}

Remarks

The type indicated here can be used with Keysight.SA.Vsa.Mode.GetConfiguration``1 to retrieve the configuration with access to configuration-specific members. It is chosen at creation (ModeCollection.Create) and does not change.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also