Returns this Mode's
ModeConfiguration cast to the requested type.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Function GetConfiguration(Of T As ModeConfiguration)() As T |
Type Parameters
- T
- The type to which to cast the returned configuration.
Return Value
This Mode's
ModeConfiguration cast to the requested type, or null if its configuration is not of the requested type.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also