Keysight 89600 VSA .NET API
Preset Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.Vsa Namespace > Mode Class : Preset Method


Glossary Item Box

Set Mode state to default values.

Syntax

Visual Basic (Declaration) 
Public MustOverride Sub Preset() 
C# 
public abstract void Preset()
C++/CLI 
public:
abstract void Preset(); 

Remarks

The mode configuration type and name is not changed as a result of this operation, and measurement associations are kept. Mode parameters are stored in the measurements the Mode drives, so the defaults are written through to every associated measurement.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also