Keysight 89600 VSA .NET API
MarkerIndex Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.Vsa Namespace > TraceMarkerEventDataSourceExtension Class : MarkerIndex Property


Glossary Item Box

Gets or sets the Agilent.SA.Vsa.Marker index from the Agilent.SA.Vsa.Trace.Markers collection.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property MarkerIndex As Integer
C# 
public abstract int MarkerIndex {get; set;}
C++/CLI 
public:
abstract property int MarkerIndex {
   int get();
   void set (    int value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also