Keysight 89600 VSA .NET API
RemoveAt Method
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > AllocationCollection Class : RemoveAt Method


index
Zero-based index of Allocation to remove from the collection

Glossary Item Box

Removes the allocation at the indicated index from the collection.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function RemoveAt( _
   ByVal index As Integer _
) As Boolean
C# 
public abstract bool RemoveAt( 
   int index
)
C++/CLI 
public:
abstract bool RemoveAt( 
   int index
) 

Parameters

index
Zero-based index of Allocation to remove from the collection

Return Value

True, if the Allocation was removed from the collection.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also