Keysight 89600 VSA .NET API
Include Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > Channel Class : Include Property


Glossary Item Box

Gets or sets a value indicating whether the channel is included in EVM calculations and shown in traces.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property Include As Boolean
C# 
public abstract bool Include {get; set;}
C++/CLI 
public:
abstract property bool Include {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true for PUSCH channel and DownlinkUser, and false for PUCCH, SRS and PRACH channels.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also