| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property IsMcsIndexCoupled As Boolean | |
| C# | |
|---|---|
public virtual bool IsMcsIndexCoupled {get; set;} | |
Property Value
The default value is true.If true, the MCS Index values defined for the individual allocations are ignored and the MCS Index value of the Channel is applied to all allocations.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 20.00