Keysight 89600 VSA .NET API
Create Method
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > DownlinkRateMatchPatternCollection Class : Create Method


Glossary Item Box

Creates and appends a rate match pattern using the lowest unused ID.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function Create() As DownlinkRateMatchPattern
C# 
public abstract DownlinkRateMatchPattern Create()
C++/CLI 
public:
abstract DownlinkRateMatchPattern^ Create(); 

Return Value

The new rate match pattern, or null when the collection already contains eight patterns.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also