The following tables list the members exposed by DownlinkRateMatchPatternCollection.
| Name | Description | Minimum SW Version | |
|---|---|---|---|
![]() | Count | Gets the number of items in the collection. (Inherited from Agilent.SA.Vsa.RemotableCollection<DownlinkRateMatchPattern>) | — |
![]() | IsDisposed | Gets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | Item | Get the item at a specified index. (Inherited from Agilent.SA.Vsa.RemotableCollection<DownlinkRateMatchPattern>) | — |
| ‡ This is the minimum 89600 VSA software version level needed to use this member. | |||
| Name | Description | Minimum SW Version | |
|---|---|---|---|
![]() | Clear | Removes all patterns and restores one disabled pattern with ID 0. | — |
![]() | Create | Creates and appends a rate match pattern using the lowest unused ID. | — |
![]() | CreateObjRef | Creates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject) | — |
![]() | ForceRebuildKeyMap | This method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | GetEnumerator | Gets an enumerator for the collection. (Inherited from Agilent.SA.Vsa.RemotableCollection<DownlinkRateMatchPattern>) | — |
![]() | GetLifetimeService | Retrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject) | — |
![]() | IndexOf | Overloaded. Gets the index location of the specified item within the collection. (Inherited from Agilent.SA.Vsa.RemotableCollection<DownlinkRateMatchPattern>) | — |
![]() | InitializeLifetimeService | Obtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | Remove | Removes a rate match pattern from the collection. | — |
![]() | RemoveAt | Removes the rate match pattern at the specified zero-based collection index. | — |
| ‡ This is the minimum 89600 VSA software version level needed to use this member. | |||
| Name | Description | Minimum SW Version | |
|---|---|---|---|
![]() | CollectionChanged | Occurs when an item is added, removed, changed, moved, or the entire list is refreshed. (Inherited from Agilent.SA.Vsa.RemotableCollection<DownlinkRateMatchPattern>) | — |
![]() | PropertyChanged | Occurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | PropertyInfoChanged | Occurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | RemoteCollectionChanged | Occurs when an item is added, removed, changed, moved, or the entire list is refreshed. (Inherited from Agilent.SA.Vsa.RemotableCollection<DownlinkRateMatchPattern>) | 14.00 |
![]() | RemotePropertyChanged | Occurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | RemotePropertyInfoChanged | Occurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | 14.00 |
| ‡ This is the minimum 89600 VSA software version level needed to use this member. | |||