Keysight 89600 VSA .NET API
AntennaDetectionThreshold Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : AntennaDetectionThreshold Property


Glossary Item Box

Gets or sets the antenna detection threshold in dB relative to the reference path.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property AntennaDetectionThreshold As Double
C# 
public abstract double AntennaDetectionThreshold {get; set;}
C++/CLI 
public:
abstract property double AntennaDetectionThreshold {
   double get();
   void set (    double value);
}

Property Value

The default value is -36 dB. The minimum value is -100dB and the maximum is 100 dB.

Remarks

Channel paths whose power level fall below this threshold are not detected.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also