Keysight 89600 VSA .NET API
MeasurementExtension Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : MeasurementExtension Class

Glossary Item Box

The following tables list the members exposed by MeasurementExtension.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyAnalysisBandwidthGets or sets the analysis bandwidth.  —
Public PropertyAnalysisStartBoundaryGets or sets the analysis start boundary.  —
Public PropertyAntennaArrayShapeGets or sets the Antenna Array Shape.  22.20
Public PropertyAntennaDetectionThresholdGets or sets the antenna detection threshold in dB relative to the reference path.  —
Public PropertyAntennaElementSpacingGets or sets what the spacing between antenna elements is in terms of the signal wavelength.  —
Public PropertyAntennaElementSpacingXGets or sets what the spacing between antenna elements is in terms of the signal wavelength.  22.20
Public PropertyAntennaElementSpacingYGets or sets what the spacing between antenna elements is in terms of the signal wavelength.  22.20
Public PropertyBeamPatternDisplayGroupIndexGets or sets the antenna group index of the beam forming trace.  22.20
Public PropertyBeamPatternDisplayHorizontalAngleGets or sets the horizontal angle of the plane displayed in the beam forming trace.  22.20
Public PropertyBeamPatternDisplayLayerIndexGets or sets the antenna layer index of the beam forming trace.  22.20
Public PropertyBeamPatternDisplayPeakUEGets or sets the index of the UE whose peak beam angle on this layer is used to cut the 3D trace and show it in 2D trace.  22.20
Public PropertyBeamPatternDisplayVerticalAngleGets or sets the vertical angle of the plane displayed in the beam forming trace.  22.20
Public PropertyCellBeamDirectionPhiGets or sets the horizontal angle of the cell beam direction (Downlink only).  23.20
Public PropertyCellBeamDirectionThetaGets or sets the vertical angle of the cell beam direction (Downlink only).  23.20
Public PropertyCellBeamSeparationMethodGets or sets the cell separation method (Downlink only).  23.20
Public PropertyCellIdentityGets or sets the Physical Layer Cell ID.  —
Public PropertyCellIdModeGets or sets the Cell ID Mode as being auto-detected or manually detected (Downlink only).  —
Public PropertyChannelConditionGets or sets the channel condition to be used for spectral flatness test as normal or extreme.  15.00
Public PropertyCrcDecodeMaxIterationCountGets or sets the maximum number of LTE turbo decoder iterations to perform when determining a CRC pass result before returning a CRC fail result.  29.40
Public PropertyCsiRsScaleFactorGets or sets the per-subcarrier CSI-RS scale factor in dB.  16.00
Public PropertyCyclicPrefixLengthModeGets or sets the Cyclic Prefix length mode as being auto-detected, normal or extended.  —
Public PropertyDciFormat1BPuschPmiReport1LayerGets or sets the latest PMI report on PUSCH for 1 layer DCI Format 1B scheduled allocations.  14.00
Public PropertyDciFormat1Format1ADetectGets or sets whether a PDCCH with ambiguous length is to be decoded as DCI Format 1 or Format 1A  19.00
Public PropertyDciFormat2PuschPmiReport1LayerGets or sets the latest PMI report on PUSCH for 1 layer DCI Format 2 scheduled allocations.  14.00
Public PropertyDciFormat2PuschPmiReport2LayerGets or sets the latest PMI report on PUSCH for 2 layer DCI Format 2 scheduled allocations.  14.00
Public PropertyDciFormat2PuschPmiReport3LayerGets or sets the latest PMI report on PUSCH for 3 layer DCI Format 2 scheduled allocations.  14.00
Public PropertyDciFormat2PuschPmiReport4LayerGets or sets the latest PMI report on PUSCH for 4 layer DCI Format 2 scheduled allocations.  14.00
Public PropertyDownlinkMultipleAccessSchemeGets or sets the multiple access scheme used for Downlink  21.00
Public PropertyDownlinkPilotPrsGets or sets the downlink RS PRS type (Downlink only).  —
Public PropertyDownlinkRateMatchPatternsGets the downlink rate match pattern configurations for O-RAN Fronthaul WG4 testing. Returns null when the host implementation does not support rate match pattern configuration. See DownlinkRateMatchPatternCollection for full semantics.  31.00
Public PropertyDownlinkRsScaleFactorGets or sets the per-subcarrier DL RS scale factor in dB.  14.00
Public PropertyDownlinkSynchronizationSlotIndexGets or sets the Downlink synchronization slot index.  21.00
Public PropertyDownlinkUsersGets the collection of downlink users (PDSCH channels).  —
Public PropertyDuplexModeGets or sets the Duplex Mode (FDD or TDD).  —
Public PropertyElementSpacingUnitGets or sets the Element Spacing Unit.  22.20
Public PropertyEnableMultiplePciSeparationGets or sets a value indicating whether to enable multiple PCIs separation(Downlink only).  23.20
Public PropertyEqualizerTrainingGets or sets the equalizer training type as being Off or RS-based or RS+Data based.  —
Public PropertyEqualizerTrainingModeGets or sets the equalizer training mode (Uplink only)  —
Public PropertyEqualizerTrainingMovingAverageLengthGets or sets the EQ Moving Average Filter Length in RS subcarriers.  —
Public PropertyEvmMinimizationGets or sets what EVM Minimization method is employed.  —
Public PropertyEvmTransientLaggingTimeLengthGets or sets the lagging time length for EVM transient time exclusion.  —
Public PropertyEvmTransientLeadingTimeLengthGets or sets the leading time length for EVM transient time exclusion.  —
Public PropertyEvmTransientPowerChangeTimeLengthGets or sets the time length for EVM transient time exclusion when the power change between PUSCH slots exceeds the power ratio threshold.  —
Public PropertyEvmTransientTimePowerRatioThresholdGets or sets the power ratio threshold for transition between PUSCH slots that will trigger EVM transient time exclusion.  —
Public PropertyEvmWindowLengthModeGets or sets the EVM Window Length mode as being 3GPP standard-defined or custom-defined  —
Public PropertyEvmWindowLengthSampleGets or sets the EVM Window Length in samples.  —
Public PropertyExpectedNumberOfDLUsersGets or sets the expected maximum number of users within the meas. interval (only for PDCCH-decode based auto-detection)  —
Public PropertyFofdmFilterGets or sets the filter method used for F-OFDM  21.00
Public PropertyFofdmFilterCoefficientsGets or sets the filter coefficients for F-OFDM filtering  21.00
Public PropertyFofdmFilterLengthGets or sets the filter length used for F-OFDM  21.00
Public PropertyFofdmFilterSamplingFrequencyGets or sets the sampling frequency of the filter coefficients used for F-OFDM  21.00
Public PropertyFofdmFilterWindowGets or sets the filter method used for F-OFDM  21.00
Public PropertyFofdmFilterWindowLengthModeGets or sets the window filter length mode used for F-OFDM  21.00
Public PropertyFofdmPassbandBWGets or sets the passband bandwidth of F-OFDM subband  21.00
Public PropertyFofdmPassbandRippleGets or sets the passband ripple of F-OFDM subband  21.00
Public PropertyFofdmStopbandAttenuationGets or sets the stopband attenuation of F-OFDM subband  21.00
Public PropertyFofdmTransitionBWGets or sets the transition bandwidth of F-OFDM subband  21.00
Public PropertyFrequencyCenterULGets or sets the center frequency of the UL signal, to be used to determine the limits for UL spectrum flatness test.  15.00
Public PropertyFrequencyHighULGets or sets the highest frequency of the UL operating band.  15.00
Public PropertyFrequencyLowULGets or sets the lowest frequency of the UL operating band.  15.00
Public PropertyFrequencyOffsetGets or sets the frequency offset of the component carrier from the measurement center frequency, if the carrier is a component carrier of LTE-Advanced  14.00
Public PropertyInputChannelGets or sets the reference measurement input channel.  —
Public PropertyInputChannelIncludeGets or sets the array of booleans to indicate which measurement input channels belong to the carrier, if the carrier is a component carrier of LTE-Advanced  15.00
Public PropertyInterferenceCellIdGets or sets the Cell ID of the second cell (Downlink only).  23.20
Public PropertyIsAmplitudeIncludedInEvmMinimizationGets or sets a value indicating whether EVM Minimization of Amplitude is enabled.  —
Public PropertyIsBeamPatternDisplayPeakUEGets or sets a value indicating whether to enable the specified UE's peak beam angle on the specified layer to cut the 3D trace and show it in 2D trace.  22.20
Public PropertyIsCarrierAllocatedGets or sets a value indicating whether the component carrier is an allocated carrier.  19.00
Public PropertyIsCarrierIndicatorFieldPresentGets or sets a value indicating whether the Carrier Indicator Field is present in the DCI messages.  19.00
Public PropertyIsControlChannelPowerLevelAutoDetectedGets or sets a value indicating whether DL control channels' power levels are auto-detected  17.00
Public PropertyIsCrossCarrierSchedulingEnabledGets or sets a value indicating whether cross-carrier scheduling is enabled. The property indicates whether the carrier's allocations are defined in its own PDCCH or in another carrier's PDCCH.  19.00
Public PropertyIsCsiRsActiveGets or sets a value indicating whether CSI-RS is present in the signal, if the carrier is a component carrier of LTE-Advanced  16.00
Public PropertyIsCsiRsEnabledGets or sets a value indicating whether CSI-RS is enabled in trace displays and included in overall EVM calculation.  16.00
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyIsEMTCAnalysisGets or sets a value indicating whether the uplink measurement is for an eMTC uplink measurement. if this value is true and the LinkDirection is uplink, the active uplink channels will be processed as eMTC uplink channels.  21.20
Public PropertyIsEqualizerChannelFrequencyResponseNormalizedGets or sets a value indicating whether EQ Channel Frequency Response is normalized.  —
Public PropertyIsEqualizerTrainingMovingAverageEnabledGets or sets a value indicating whether Moving Average is employed in equalizer training  —
Public PropertyIsEvmReportedInDBGets or sets a value indicating whether EVM results are reported in dB.  —
Public PropertyIsEvmTransientTimeExcludedGets or sets a value indicating whether EVM transient time is excluded from EVM calculations  —
Public PropertyIsFrameTriggerOnGets or sets a value indicating whether to enable the frame trigger.  22.20
Public PropertyIsFreqLockRangeExtendedGets or sets a value indicating whether Frequency Lock Range is extended.  —
Public PropertyIsFrequencyIncludedInEvmMinimizationGets or sets a value indicating whether EVM Minimization of frequency is enabled.  —
Public PropertyIsFrequencyMirroredGets or sets a value indicating whether demod will mirror the frequency spectrum.  —
Public PropertyIsHalfSubcarrierShiftEnabledGets or sets a value indicating whether UL half subcarrier shift is enabled.  —
Public PropertyIsHigherOrderModulationEnabledGets or sets a value indicating whether higher order modulation (256 QAM) is enabled  20.00
Public PropertyIsInactiveEnabledGets or sets a value indicating whether non-allocated channels are enabled in trace displays and included in overall EVM calculation.  —
Public PropertyIsIncludeInactivePathsEnabledGets or sets a value indicating whether antenna paths below the antenna detection threshold (-36 dB default) in power from the reference antenna path are shown or blanked on the MIMO traces.  —
Public PropertyIsIQOffsetIncludedInEvmMinimizationGets or sets a value indicating whether EVM Minimization of IQ Offset is enabled.  —
Public PropertyIsMbsfnActiveGets or sets a value indicating whether the signal has an MBSFN region  15.00
Public PropertyIsMbsfnRsEnabledGets or sets a value indicating whether MBSFN-RS is enabled in trace displays and included in overall EVM calculation.  15.00
Public PropertyIsMulticarrierFilterEnabledGets or sets a value indicating whether multi-carrier filter will be applied.  —
Public PropertyIsOppositeDirectionPresentGets or sets a value indicating whether downlink slots are occupied when analyzing uplink in TDD, and vice-versa.  —
Public PropertyIsPbchEnabledGets or sets a value indicating whether PBCH is enabled in trace displays and included in overall EVM calculation.  —
Public PropertyIsPcfichActiveGets or sets a value indicating whether PCFICH is present in the signal.  28.00
Public PropertyIsPcfichEnabledGets or sets a value indicating whether PCFICH is enabled in trace displays and included in overall EVM calculation.  —
Public PropertyIsPdcchAllocationAutoDetectedGets or sets a value indicating whether PDCCH Symbol Allocations can be auto-detected from PCFICH  —
Public PropertyIsPdcchAllocationConstantGets or sets a value indicating whether PDCCH Symbol Allocations is constant for all sub-frames or not.  —
Public PropertyIsPdcchEnabledGets or sets a value indicating whether PDCCH is enabled in trace displays and included in overall EVM calculation.  —
Public PropertyIsPhichActiveGets or sets a value indicating whether PHICH is present in the signal.  28.00
Public PropertyIsPhichDespreadGets or sets a value indicating whether PHICH Despread IQ is enabled.  —
Public PropertyIsPhichEnabledGets or sets a value indicating whether PHICH is enabled in trace displays and included in overall EVM calculation.  —
Public PropertyIsPmchEnabledGets or sets a value indicating whether PMCH is enabled in trace displays and included in overall EVM calculation.  15.00
Public PropertyIsPositioningRsActiveGets or sets a value indicating whether Positioning RS is present in the signal.  15.00
Public PropertyIsPositioningRsEnabledGets or sets a value indicating whether Positioning RS is enabled in trace displays and included in overall EVM calculation.  15.00
Public PropertyIsPowerBoostNormalizedGets or sets a value indicating whether channels' power levels are normalized to 0dB in traces.  —
Public PropertyIsPowerLevelAutoDetectedGets or sets a value indicating whether DL power levels are auto-detected (only for PDCCH-decode based auto-detection)  —
Public PropertyIsPowerLevelAutoDetectedInPowerModeGets or sets a value indicating whether DL power levels are auto-detected (only for power-based auto-detection)  —
Public PropertyIsPowerRoundedToStandardGets or sets a value indicating whether the auto-detected power levels are rounded to the nearest standard-defined levels (only for PDCCH-decode based auto-detection)  —
Public PropertyIsPschEnabledGets or sets a value indicating whether P-SS is enabled in trace displays and included in overall EVM calculation.  —
Public PropertyIsPSDCHActiveGets or sets a value indicating whether PSDCH is active to indicate the traffic channel is PUSCH(physical uplink shared channel) or PSDCH(physical side-link discovery channel) if this value is true and the LinkDirection is uplink, the active channel will be processed as PSDCH.  21.00
Public PropertyIsPucchCqiPmiInformationSizeAutoDetectedGets or sets a value indicating whether PUCCH CQI/PMI Info Size Auto is enabled.  —
Public PropertyIsPucchHarqAckInformationSizeAutoDetectedGets or sets a value indicating whether PUCCH HARQ-ACK Info Size Auto is enabled.  —
Public PropertyIsPuschCqiPmiInformationSizeAutoDetectedGets or sets a value indicating whether PUSCH CQI/PMI Info Size Auto is enabled.  —
Public PropertyIsPuschCqiPmiInformationSizeDynamicGets or sets a value indicating whether PUSCH CQI/PMI Info Size can be dynamically changing between any two PUSCH subframe allocations.  30.00
Public PropertyIsPuschDftSwapEnabledGets or sets a value indicating whether PUSCH DFT Swap is enabled.  —
Public PropertyIsPuschHarqAckInformationSizeAutoDetectedGets or sets a value indicating whether PUSCH HARQ-ACK Info Size Auto is enabled.  —
Public PropertyIsPuschHarqAckInformationSizeDynamicGets or sets a value indicating whether PUSCH HARQ-ACK Info Size can be dynamically changing between any two PUSCH subframe allocations.  30.00
Public PropertyIsPuschRIInformationSizeAutoDetectedGets or sets a value indicating whether PUSCH RI Info Size Auto is enabled.  —
Public PropertyIsPuschRIInformationSizeDynamicGets or sets a value indicating whether PUSCH RI Info Size can be dynamically changing between any two PUSCH subframe allocations.  30.00
Public PropertyIsQam1024EnabledGets or sets a value indicating whether 1024 QAM is enabled  24.00
Public PropertyIsRBAutoDetectGets or sets a value indicating whether Auto-Detection of user allocations is enabled.  —
Public PropertyIsRSEnabledGets or sets a value indicating whether RS is enabled in trace displays and included in overall EVM calculation (Downlink only).  —
Public PropertyIsSschEnabledGets or sets a value indicating whether S-SS is enabled in trace displays and included in overall EVM calculation.  —
Public PropertyIsTimingIncludedInEvmMinimizationGets or sets a value indicating whether EVM Minimization of Timing is enabled.  —
Public PropertyIsTwoFrameAnalysisEnabledGets or sets a value indicating whether Two-Frame analysis of user allocations is enabled.  —
Public PropertyIsUersChannelResponseCompensationEnabledGets or sets a value indicating whether channel response is compensated from UE-RS weights  —
Public PropertyIsUersWeightsInRealImaginaryEnabledGets or sets a value indicating whether UE-specific RS weights displayed in the UE-specific RS weights table are in Real/Imaginary format  —
Public PropertyIsULPowerLevelAutoDetectedGets or sets a value indicating whether UL power levels are auto-detected.  —
Public PropertyIsUsePerAntennaEpreGets or sets a value indicating whether the Per-antenna EPRE is used or the CW0/CW1 Power Boost is used to specify the power levels of users/allocations  15.00
Public PropertyIsUseRelativePowerLevelsEnabledGets or sets a value indicating whether results are reported using relative power levels.  —
Public PropertyLinkDirectionGets or sets the link direction.  —
Public PropertyMbsfnAreaIdGets or sets the MBSFN Area ID.  15.00
Public PropertyMbsfnRsScaleFactorGets or sets the per-subcarrier scale factor of MBSFN-RS in dB.  15.00
Public PropertyMeasureIntervalSlotsGets or sets the measurement interval as an integer number of slots.  —
Public PropertyMeasureIntervalSymbolsGets or sets the measurement interval as an integer number of symbols.  —
Public PropertyMeasureOffsetSlotsGets or sets the measurement offset expressed as an integer number of slots.  —
Public PropertyMeasureOffsetSymbolsGets or sets the measurement offset expressed as an integer number of symbol times.  —
Public PropertyMimoDecodingGets or sets the MIMO decoding to apply to channels that have undergone MIMO precoding.  —
Public PropertyMUSTCategoryGets or sets the multiuser superposition transmission scheme  21.00
Public PropertyMUSTSICModeGets or sets the signal interference cancellation method used for multiuser superposition transmission measurement  21.00
Public PropertyNameGets the name of the carrier, if it is a component carrier of LTE-Advanced  14.00
Public PropertyNonMbsfnRegionLengthGets or sets the length of the non-MBSFN region in symbols within the MBSFN sub-frames.  15.00
Public PropertyNonzeroCsiRsConfigurationGets or sets the CSI-RS configuration.  16.00
Public PropertyNonzeroCsiRsSubframeConfigurationGets or sets the CSI-RS subframe configuration.  16.00
Public PropertyNumberOfCsiRsPortsGets or sets the number of antenna ports used for CSI-RS transmission  16.00
Public PropertyNumberOfElementsPerAntennaGroupGets or sets the number of antenna elements within each beam forming Antenna Group.  15.00
Public PropertyNumberOfElementsPerAntennaGroupXGets or sets the number of antenna elements within each beam forming Antenna Group.  22.20
Public PropertyNumberOfElementsPerAntennaGroupYGets or sets the number of antenna elements within each beam forming Antenna Group.  22.20
Public PropertyNumberOfPositioningRsSubframesGets or sets the number of consecutive downlink sub-frames (N_PRS) in which P-RS is transmitted.  15.00
Public PropertyNumberOfTXAntennasGets or sets the number of TX Antenna ports that the signal uses.  —
Public PropertyPbchBitVectorSelectGets or sets the PBCH Bit Vector Selection to be applied.  —
Public PropertyPbchScaleFactorGets or sets the per-subcarrier PBCH scale factor in dB.  —
Public PropertyPcfichBitVectorSelectGets or sets the PCFICH Bit Vector Selection to be applied.  —
Public PropertyPcfichScaleFactorGets or sets the per-subcarrier PCFICH scale factor in dB.  —
Public PropertyPdcchBitVectorSelectGets or sets the PDCCH Bit Vector Selection to be applied.  —
Public PropertyPdcchScaleFactorGets or sets the per-subcarrier PDCCH scale factor in dB.  —
Public PropertyPdcchScaleFactorIncrementGets or sets the per-subcarrier PDCCH scale factor increment in dB.  23.20
Public PropertyPdschBitVectorSelectGets or sets the PDSCH Bit Vector Selection to be applied.  —
Public PropertyPdschCellSpecificRatioGets or sets the PDSCH Cell Specific Ratio to be applied.  —
Public PropertyPdschIQReferenceGenerationModeGets or sets the reference IQ constellation mode for PDSCH  20.00
Public PropertyPdschStartOfdmSymbolGets or sets the starting OFDM symbol of PDSCH for the concerned SCell.  19.00
Public PropertyPhichAllocationGets or sets the PHICH Allocation size to be used for PHICH resource element group mappings.  —
Public PropertyPhichDurationModeGets or sets the PHICH Duration mode as being auto-detected, normal or extended.  —
Public PropertyPhichMIDefinitionGets or sets the definition of m(i) to define the specific PHICH configuration for different sub-frames (TDD only).  —
Public PropertyPhichScaleFactorGets or sets the per-subcarrier PHICH scale factor in dB.  —
Public PropertyPhichScaleFactorIncrementGets or sets the per-subcarrier PHICH scale factor increment in dB.  23.20
Public PropertyPositioningRsBandwidthGets or sets Positioning RS Bandwidth, N_RB^PRS.  15.00
Public PropertyPositioningRsConfigIndexGets or sets the Positioning RS configuration index.  15.00
Public PropertyPositioningRsPrecodingGets or sets whether the signal has precoding applied to the Positioning RS resource elements.  16.00
Public PropertyPositioningRsScaleFactorGets or sets the per-subcarrier Positioning RS scale factor in dB.  15.00
Public PropertyPschScaleFactorGets or sets the per-subcarrier P-SS scale factor in dB.  —
Public PropertyPucchBitVectorSelectGets or sets the PUCCH Bit Vector Selection to be applied.  —
Public PropertyPucchCqiPmiInformationSizeGets or sets the PUCCH CQI/PMI Info Size.  —
Public PropertyPucchHarqAckInformationSizeGets or sets the PUCCH HARQ-ACK Info Size.  —
Public PropertyPuschBitVectorSelectGets or sets the PUSCH Bit Vector Selection to be applied.  —
Public PropertyPuschCqiPmiInformationSizeGets or sets the PUSCH CQI/PMI Info Size  —
Public PropertyPuschCqiPmiOffsetIndexGets or sets the PUSCH CQI/PMI Offset Index.  —
Public PropertyPuschHarqAckInformationSizeGets or sets the PUSCH HARQ-ACK Info Size.  —
Public PropertyPuschHarqAckOffsetIndexGets or sets the PUSCH HARQ-ACK Offset Index.  —
Public PropertyPuschRIInformationSizeGets or sets the PUSCH RI Info Size.  —
Public PropertyPuschRIOffsetIndexGets or sets the PUSCH RI Offset Index.  —
Public PropertyPuxchTddAckNackFeedbackModeGets or sets the TDD PUSCH/PUCCH Ack/Nack Feedback Mode to be applied.  —
Public PropertyRARntiRangeMaxValueGets or sets the maximum value of RA-RNTI Range  —
Public PropertyRARntiRangeMinValueGets or sets the minimum value of RA-RNTI Range  —
Public PropertyRBAutoDetectModeGets or sets a value indicating whether RB Auto Detection is power-based or PDCCH-decode-based  —
Public PropertyRBPowerDetectionThresholdGets or sets the RB Power detection threshold in dB relative to the CRS power for Downlink measurement. Gets or sets the RB Power detection threshold in dB relative to the peak RB power for uplink measurement.  21.20
Public PropertyResultLengthGets or sets the result length (in slots).  —
Public PropertySchedulingCellIdGets or sets the serving cell index of the carrier whose PDCCH contains the allocations for this SCell.  19.00
Public PropertyScmaCodebookGets or sets the codebook for SCMA  21.00
Public PropertyScmaCodeWordSizeGets or sets the code-word size for SCMA  21.00
Public PropertyScmaEnabledLayersGets or sets the enabled layer for SCMA  21.0
Public PropertyScmaNumberOfLayersGets or sets the number of layers for SCMA  21.00
Public PropertyScmaSpreadingFactorGets or sets the spreading factor (number of REs over which each symbol is spread) for SCMA  21.00
Public PropertyServingCellIndexGets or sets the serving cell index.  19.00
Public PropertySpecialSubframeConfigurationGets or sets the Dw/GP/Up Length for TDD.  —
Public PropertySschScaleFactorGets or sets the per-subcarrier S-SS scale factor in dB.  —
Public PropertySymbolTimeAdjustmentGets or sets where within the cyclic prefix IFFT begins as a percentage of the IFFT duration.  —
Public PropertySymbolTimeAdjustmentModeGets or sets the Symbol Time Adjust mode.  —
Public PropertySynchronizationSignalAntennaPortGets or sets the P-SS/S-SS Antenna Port or Ports used for synchronization signal transmission.  —
Public PropertySynchronizationSignalPrecodingGets or sets whether the signal has precoding applied to the sync signals' (PSS/SSS) resource elements.  20.00
Public PropertySynchronizationTypeGets or sets the channel to synchronize to.  —
Public PropertyTimeScaleFactorGets or sets the time scale factor.  —
Public PropertyTpcRntiRangeMaxValueGets or sets the maximum value of TPC-RNTI Range  —
Public PropertyTpcRntiRangeMinValueGets or sets the minimum value of TPC-RNTI Range  —
Public PropertyTransmissionModeIncludeGets or sets which Transmission Modes are to be included in the detection of DCI Formats.  19.00
Public PropertyTXAntennaGets or sets the TX antenna port to be used as the reference antenna port  —
Public PropertyUersWeightsDisplayModeGets or sets how the UE-specific RS weights are displayed in the UE-specific RS weights table.  —
Public PropertyUplinkBandwidthForDciDecodingGets or sets the uplink bandwidth to be used in decoding certain DCI Formats.  19.00
Public PropertyUplinkDownlinkAllocationGets or sets the Uplink/Downlink configuration type for TDD.  14.00
Public PropertyUplinkEMTCCEModeGets or sets the coverage enhancement mode used by eMTC. this parameter needs to be set when the IsEMTCAnalysis is true  21.20
Public PropertyUplinkEMTCPuschAbsSubframeNumberGets or sets the number of absolute subframes over which PUSCH repeats. this parameter needs to be set when the IsEMTCAnalysis is true  21.20
Public PropertyUplinkEMTCSubframeNumberGets or sets the number of consecutive absolute subframes over which PUCCH or PUSCH stays at the same narrow band before hopping to another narrow band, expressed as a number of absolute subframes. this parameter needs to be set when the IsEMTCAnalysis is true  21.20
Public PropertyUplinkMultipleAccessSchemeGets or sets the multiple access scheme used for Uplink  21.00
Public PropertyUplinkUsersGets the collection of uplink users.  —
Public PropertyUseAntennaGets or sets a value indicating whether to use the user-specified Tx antenna port as reference  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public Methodstatic (Shared in Visual Basic)CastToExtensionTypeThis method casts the supplied object to the MeasurementExtension type. Some tools are unable to use the generic methods provided on Agilent.SA.Vsa.Measurement class so this is provided as an alternative.  —
Public MethodCopyAutoToManualCopy auto-detected allocations over to manual allocations  —
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodExportFofdmFilterCoefficientsExport filter coefficients of F-OFDM filtering  21.00
Public MethodExportLteSettingsExport only LTE setup parameters to a setup file  18.00
Public MethodExportScmaCodebookExport SCMA Codebook  21.00
Public Methodstatic (Shared in Visual Basic)ExtensionTypeReturns the type for instances this measurement extension. Some tools are unable to use the generic methods provided on Agilent.SA.Vsa.Measurement class so this is provided as an alternative.  —
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetIsPmchPresentGets whether the indicated subframe contains a PMCH transmission.  15.00
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodGetMbsfnSubframeConfigGets whether the indicated subframe is an MBSFN subframe.  15.00
Public MethodGetPdcchAllocationGet the number of PDCCH symbols allocated in the indicated subframe.  —
Public MethodGetPhaseOffsetCorrectionGet the phase offset of measurement input channel relative to the reference InputChannel in degrees.  15.00
Public MethodGetPmchModTypeGets the mod type of PMCH contained in the indicated subframe.  15.00
Public MethodGetPmchScaleFactorGets the per-subcarrier scale factor of PMCH in dB, present in the indicated subframe  15.00
Public MethodImportFofdmFilterCoefficientsImport filter coefficients of F-OFDM filtering  21.00
Public MethodImportLteSettingsOverloaded. Import only LTE setup parameters from a setup file  —
Public MethodImportScmaCodebookImport SCMA Codebook  21.00
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodPresetPreset all measurement attributes to their defaults for the indicated bandwidth  —
Public MethodSetIsPmchPresentSets whether the specified subframe contains a PMCH transmission.  15.00
Public MethodSetMbsfnSubframeConfigSets whether the specified subframe is an MBSFN subframe.  15.00
Public MethodSetPdcchAllocationSet the number of PDCCH symbols allocated in the specified subframe.  —
Public MethodSetPhaseOffsetCorrectionSet the phase offset of measurement input channel relative to the reference InputChannel in degrees.  15.00
Public MethodSetPmchModTypeSets the mod type of the PMCH contained in the indicated subframe.  15.00
Public MethodSetPmchScaleFactorSets the per-subcarrier scale factor of PMCH in dB present in the indicated subframe  15.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also