Keysight 89600 VSA .NET API
AntennaElementSpacingX Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : AntennaElementSpacingX Property


Glossary Item Box

Gets or sets what the spacing between antenna elements is in terms of the signal wavelength.

Syntax

Visual Basic (Declaration) 
Public Overridable Property AntennaElementSpacingX As Single()
C# 
public virtual float[] AntennaElementSpacingX {get; set;}
C++/CLI 
public:
virtual property array<float>^ AntennaElementSpacingX {
   array<float>^ get();
   void set (    array<float>^ value);
}

Property Value

The default value is 0.5. The minimum value is 0 and the maximum is 100.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 22.20

See Also