Gets or sets what the spacing between antenna elements is in terms of the signal wavelength.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property AntennaElementSpacingY As Single() |
| C# | |
|---|
public virtual float[] AntennaElementSpacingY {get; set;} |
Property Value
The default value is 0.5. The minimum value is 0 and the maximum is 100.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 22.20
See Also