Keysight 89600 VSA .NET API
BeamPatternDisplayPeakUE Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : BeamPatternDisplayPeakUE Property


Glossary Item Box

Gets or sets the index of the UE whose peak beam angle on this layer is used to cut the 3D trace and show it in 2D trace.

Syntax

Visual Basic (Declaration) 
Public Overridable Property BeamPatternDisplayPeakUE As Integer
C# 
public virtual int BeamPatternDisplayPeakUE {get; set;}
C++/CLI 
public:
virtual property int BeamPatternDisplayPeakUE {
   int get();
   void set (    int value);
}

Property Value

The default value is 0.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 22.20

See Also