Keysight 89600 VSA .NET API
CellBeamDirectionPhi Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : CellBeamDirectionPhi Property


Glossary Item Box

Gets or sets the horizontal angle of the cell beam direction (Downlink only).

Syntax

Visual Basic (Declaration) 
Public Overridable Property CellBeamDirectionPhi As Double
C# 
public virtual double CellBeamDirectionPhi {get; set;}
C++/CLI 
public:
virtual property double CellBeamDirectionPhi {
   double get();
   void set (    double value);
}

Property Value

The default value is 0.0.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20

See Also