Keysight 89600 VSA .NET API
DownlinkPilotPrs Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : DownlinkPilotPrs Property


Glossary Item Box

Gets or sets the downlink RS PRS type (Downlink only).

Syntax

Visual Basic (Declaration) 
Public MustOverride Property DownlinkPilotPrs As PilotPrsType
C# 
public abstract PilotPrsType DownlinkPilotPrs {get; set;}
C++/CLI 
public:
abstract property PilotPrsType DownlinkPilotPrs {
   PilotPrsType get();
   void set (    PilotPrsType value);
}

Property Value

The default value is PilotPrsType.Auto.

Remarks

PilotPrsType.Custom selection is not available if SynchronizationType = SynchronizationTypeSelection.RS

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also