Gets or sets the Downlink synchronization slot index.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property DownlinkSynchronizationSlotIndex As Integer |
| C# | |
|---|
public virtual int DownlinkSynchronizationSlotIndex {get; set;} |
| C++/CLI | |
|---|
public:
virtual property int DownlinkSynchronizationSlotIndex {
int get();
void set ( int value);
} |
Property Value
The default value is 0. The minimum value is 0 and the maximum is 19.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 21.00
See Also