Keysight 89600 VSA .NET API
EqualizerTrainingMode Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : EqualizerTrainingMode Property


Glossary Item Box

Gets or sets the equalizer training mode (Uplink only)

Syntax

Visual Basic (Declaration) 
Public MustOverride Property EqualizerTrainingMode As EqualizerTrainingModeType
C# 
public abstract EqualizerTrainingModeType EqualizerTrainingMode {get; set;}
C++/CLI 
public:
abstract property EqualizerTrainingModeType EqualizerTrainingMode {
   EqualizerTrainingModeType get();
   void set (    EqualizerTrainingModeType value);
}

Property Value

The default value is EqualizerTrainingModeType.ZF.

Remarks

Determines whether equalizer coefficients are calculated based on the standard Least Squares method or non-standard Zero Forcing method

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also