Keysight 89600 VSA .NET API
EvmTransientPowerChangeTimeLength Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : EvmTransientPowerChangeTimeLength Property


Glossary Item Box

Gets or sets the time length for EVM transient time exclusion when the power change between PUSCH slots exceeds the power ratio threshold.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property EvmTransientPowerChangeTimeLength As Double
C# 
public abstract double EvmTransientPowerChangeTimeLength {get; set;}
C++/CLI 
public:
abstract property double EvmTransientPowerChangeTimeLength {
   double get();
   void set (    double value);
}

Property Value

The default value is 50 us.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also