| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property ExpectedNumberOfDLUsers As Integer | |
| C# | |
|---|---|
public abstract int ExpectedNumberOfDLUsers {get; set;} | |
Property Value
The default value is 3. The minimum value is 0 and the maximum is 49.This parameter is not used if IsPowerLevelAutoDetected is true.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)