Keysight 89600 VSA .NET API
ExportLteSettings Method
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : ExportLteSettings Method


fileName
The setup file to export LTE parameters to.

Glossary Item Box

Export only LTE setup parameters to a setup file

Syntax

Visual Basic (Declaration) 
Public MustOverride Sub ExportLteSettings( _
   ByVal fileName As String _
) 
C# 
public abstract void ExportLteSettings( 
   string fileName
)
C++/CLI 
public:
abstract void ExportLteSettings( 
   String^ fileName
) 

Parameters

fileName
The setup file to export LTE parameters to.

Remarks

This method can be used to create an LTE setup file from an LTE-Advanced component carrier's settings.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 18.00

See Also