Keysight 89600 VSA .NET API
FofdmFilterLength Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : FofdmFilterLength Property


Glossary Item Box

Gets or sets the filter length used for F-OFDM

Syntax

Visual Basic (Declaration) 
Public Overridable Property FofdmFilterLength As Integer
C# 
public virtual int FofdmFilterLength {get; set;}
C++/CLI 
public:
virtual property int FofdmFilterLength {
   int get();
   void set (    int value);
}

Property Value

The default value is 1

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.00

See Also