Keysight 89600 VSA .NET API
FofdmPassbandBW Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : FofdmPassbandBW Property


Glossary Item Box

Gets or sets the passband bandwidth of F-OFDM subband

Syntax

Visual Basic (Declaration) 
Public Overridable Property FofdmPassbandBW As Double
C# 
public virtual double FofdmPassbandBW {get; set;}
C++/CLI 
public:
virtual property double FofdmPassbandBW {
   double get();
   void set (    double value);
}

Property Value

The default value is 0

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.00

See Also