Keysight 89600 VSA .NET API
FrequencyLowUL Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : FrequencyLowUL Property


Glossary Item Box

Gets or sets the lowest frequency of the UL operating band.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property FrequencyLowUL As Double
C# 
public abstract double FrequencyLowUL {get; set;}
C++/CLI 
public:
abstract property double FrequencyLowUL {
   double get();
   void set (    double value);
}

Property Value

The default value is 1920 MHz (corresponding to E-UTRA Operating Band 1). The minimum value is 0 Hz and the maximum value is 5 GHz.

Remarks

This value is used in determining the UL spectrum flatness limits.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 15.00

See Also