Gets or sets the frequency offset of the component carrier from the measurement center frequency, if the carrier is a component carrier of LTE-Advanced
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property FrequencyOffset As Double |
| C# | |
|---|
public virtual double FrequencyOffset {get; set;} |
| C++/CLI | |
|---|
public:
virtual property double FrequencyOffset {
double get();
void set ( double value);
} |
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 14.00
See Also