Keysight 89600 VSA .NET API
ImportFofdmFilterCoefficients Method
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : ImportFofdmFilterCoefficients Method


fileName
The text file from which to import the filter coefficients

Glossary Item Box

Import filter coefficients of F-OFDM filtering

Syntax

Visual Basic (Declaration) 
Public Overridable Sub ImportFofdmFilterCoefficients( _
   ByVal fileName As String _
) 
C# 
public virtual void ImportFofdmFilterCoefficients( 
   string fileName
)
C++/CLI 
public:
virtual void ImportFofdmFilterCoefficients( 
   String^ fileName
) 

Parameters

fileName
The text file from which to import the filter coefficients

Remarks

The text file contains a CSV formatted representation of the filter coefficients.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.00

See Also