Keysight 89600 VSA .NET API
InterferenceCellId Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : InterferenceCellId Property


Glossary Item Box

Gets or sets the Cell ID of the second cell (Downlink only).

Syntax

Visual Basic (Declaration) 
Public Overridable Property InterferenceCellId As Integer
C# 
public virtual int InterferenceCellId {get; set;}
C++/CLI 
public:
virtual property int InterferenceCellId {
   int get();
   void set (    int value);
}

Property Value

The default value is 0.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20

See Also