Keysight 89600 VSA .NET API
IsBeamPatternDisplayPeakUE Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : IsBeamPatternDisplayPeakUE Property


Glossary Item Box

Gets or sets a value indicating whether to enable the specified UE's peak beam angle on the specified layer to cut the 3D trace and show it in 2D trace.

Syntax

Visual Basic (Declaration) 
Public Overridable Property IsBeamPatternDisplayPeakUE As Boolean
C# 
public virtual bool IsBeamPatternDisplayPeakUE {get; set;}
C++/CLI 
public:
virtual property bool IsBeamPatternDisplayPeakUE {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 22.20

See Also