| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property IsCrossCarrierSchedulingEnabled As Boolean | |
| C# | |
|---|---|
public virtual bool IsCrossCarrierSchedulingEnabled {get; set;} | |
This property is meaningful only if the carrier is an LTE-A carrier. Cross-carrier scheduling cannot be enabled for the PCell, i.e. the cell with the ServingCellIndex of 0.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00