Keysight 89600 VSA .NET API
IsEMTCAnalysis Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : IsEMTCAnalysis Property


Glossary Item Box

Gets or sets a value indicating whether the uplink measurement is for an eMTC uplink measurement. if this value is true and the LinkDirection is uplink, the active uplink channels will be processed as eMTC uplink channels.

Syntax

Visual Basic (Declaration) 
Public Overridable Property IsEMTCAnalysis As Boolean
C# 
public virtual bool IsEMTCAnalysis {get; set;}
C++/CLI 
public:
virtual property bool IsEMTCAnalysis {
   bool get();
   void set (    bool value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.20

See Also