Keysight 89600 VSA .NET API
IsFreqLockRangeExtended Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : IsFreqLockRangeExtended Property


Glossary Item Box

Gets or sets a value indicating whether Frequency Lock Range is extended.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsFreqLockRangeExtended As Boolean
C# 
public abstract bool IsFreqLockRangeExtended {get; set;}
C++/CLI 
public:
abstract property bool IsFreqLockRangeExtended {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Remarks

When true, provides a frequency lock range of +/-(15kHz x 2 + 7.5kHz). When false, provides a frequency lock range of +/-(7.5kHz) only, but initial sync will be faster.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also