Keysight 89600 VSA .NET API
IsIQOffsetIncludedInEvmMinimization Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : IsIQOffsetIncludedInEvmMinimization Property


Glossary Item Box

Gets or sets a value indicating whether EVM Minimization of IQ Offset is enabled.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsIQOffsetIncludedInEvmMinimization As Boolean
C# 
public abstract bool IsIQOffsetIncludedInEvmMinimization {get; set;}
C++/CLI 
public:
abstract property bool IsIQOffsetIncludedInEvmMinimization {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Remarks

This is an uplink-only parameter.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also