Keysight 89600 VSA .NET API
IsPSDCHActive Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : IsPSDCHActive Property


Glossary Item Box

Gets or sets a value indicating whether PSDCH is active to indicate the traffic channel is PUSCH(physical uplink shared channel) or PSDCH(physical side-link discovery channel) if this value is true and the LinkDirection is uplink, the active channel will be processed as PSDCH.

Syntax

Visual Basic (Declaration) 
Public Overridable Property IsPSDCHActive As Boolean
C# 
public virtual bool IsPSDCHActive {get; set;}
C++/CLI 
public:
virtual property bool IsPSDCHActive {
   bool get();
   void set (    bool value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.00

See Also