Gets or sets a value indicating whether PCFICH is present in the signal.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property IsPcfichActive As Boolean |
| C# | |
|---|
public virtual bool IsPcfichActive {get; set;} |
| C++/CLI | |
|---|
public:
virtual property bool IsPcfichActive {
bool get();
void set ( bool value);
} |
Property Value
The default is true.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 28.00
See Also