Keysight 89600 VSA .NET API
IsPdcchAllocationAutoDetected Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : IsPdcchAllocationAutoDetected Property


Glossary Item Box

Gets or sets a value indicating whether PDCCH Symbol Allocations can be auto-detected from PCFICH

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsPdcchAllocationAutoDetected As Boolean
C# 
public abstract bool IsPdcchAllocationAutoDetected {get; set;}
C++/CLI 
public:
abstract property bool IsPdcchAllocationAutoDetected {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Remarks

When true, number of PDCCH symbols per subframe will be auto detected from signal by decoding the PCFICH information content for each measured subframe. When false, user can manually specify number of PDCCH symbols per subframe

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also