Keysight 89600 VSA .NET API
IsPhichDespread Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : IsPhichDespread Property


Glossary Item Box

Gets or sets a value indicating whether PHICH Despread IQ is enabled.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsPhichDespread As Boolean
C# 
public abstract bool IsPhichDespread {get; set;}
C++/CLI 
public:
abstract property bool IsPhichDespread {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Remarks

This is a downlink only parameter. Enabling the parameter enables de-spreading of PHICH Group orthogonal Sequence codes in IQ trace results.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also