Keysight 89600 VSA .NET API
IsPositioningRsActive Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : IsPositioningRsActive Property


Glossary Item Box

Gets or sets a value indicating whether Positioning RS is present in the signal.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsPositioningRsActive As Boolean
C# 
public abstract bool IsPositioningRsActive {get; set;}
C++/CLI 
public:
abstract property bool IsPositioningRsActive {
   bool get();
   void set (    bool value);
}

Property Value

The default is false.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 15.00

See Also