Gets or sets a value indicating whether DL power levels are auto-detected (only for PDCCH-decode based auto-detection)
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property IsPowerLevelAutoDetected As Boolean |
| C# | |
|---|
public abstract bool IsPowerLevelAutoDetected {get; set;} |
| C++/CLI | |
|---|
public:
abstract property bool IsPowerLevelAutoDetected {
bool get();
void set ( bool value);
} |
Property Value
The default value is true.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also