Keysight 89600 VSA .NET API
IsRBAutoDetect Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : IsRBAutoDetect Property


Glossary Item Box

Gets or sets a value indicating whether Auto-Detection of user allocations is enabled.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsRBAutoDetect As Boolean
C# 
public abstract bool IsRBAutoDetect {get; set;}
C++/CLI 
public:
abstract property bool IsRBAutoDetect {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Remarks

Enabling the parameter enables auto-detection of user allocations based on modulation format. The results show three users corresponding to the three modulation formats.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also