Keysight 89600 VSA .NET API
IsUersWeightsInRealImaginaryEnabled Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : IsUersWeightsInRealImaginaryEnabled Property


Glossary Item Box

Gets or sets a value indicating whether UE-specific RS weights displayed in the UE-specific RS weights table are in Real/Imaginary format

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsUersWeightsInRealImaginaryEnabled As Boolean
C# 
public abstract bool IsUersWeightsInRealImaginaryEnabled {get; set;}
C++/CLI 
public:
abstract property bool IsUersWeightsInRealImaginaryEnabled {
   bool get();
   void set (    bool value);
}

Property Value

The default value is false.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also