Gets or sets a value indicating whether the Per-antenna EPRE is used or the CW0/CW1 Power Boost is used to specify the power levels of users/allocations
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property IsUsePerAntennaEpre As Boolean |
| C# | |
|---|
public abstract bool IsUsePerAntennaEpre {get; set;} |
| C++/CLI | |
|---|
public:
abstract property bool IsUsePerAntennaEpre {
bool get();
void set ( bool value);
} |
Property Value
The default value is true.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 15.00
See Also