Keysight 89600 VSA .NET API
MUSTSICMode Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : MUSTSICMode Property


Glossary Item Box

Gets or sets the signal interference cancellation method used for multiuser superposition transmission measurement

Syntax

Visual Basic (Declaration) 
Public Overridable Property MUSTSICMode As MUSTSICModeType
C# 
public virtual MUSTSICModeType MUSTSICMode {get; set;}
C++/CLI 
public:
virtual property MUSTSICModeType MUSTSICMode {
   MUSTSICModeType get();
   void set (    MUSTSICModeType value);
}

Property Value

The default value is DEMOD/>

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.00

See Also