Gets or sets the measurement interval as an integer number of slots.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property MeasureIntervalSlots As Integer |
| C# | |
|---|
public abstract int MeasureIntervalSlots {get; set;} |
| C++/CLI | |
|---|
public:
abstract property int MeasureIntervalSlots {
int get();
void set ( int value);
} |
Property Value
The default value is 2. The minimum value is 0 and the maximum is ResultLength.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also